我用ths60120差动驱动器当作功率放大器,驱动51欧电阻,输出电压有效值要求能够大于10V,正弦波输入频率能够达到10MHz。请问这块芯片能承受的了吗?实际我测试的时候在输出峰峰值达到20V时就出现失真了,而且是频率越大失真越严重。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
手册第5页指出,这颗芯片在+/-15V供电下单端的典型摆幅是-12.2V~12.5V,你如果想达到10V有效值,电压峰峰值应该在28V,明显超过芯片可承受范围。
另外,手册第5页指出Voutpp在20V时,对1MHz信号的THD只有-65dBc。当信号频率增加时,THD肯定是下降的,所以对于10MHz的输入,THD应该到不了-65dBc,在大电压输出下,很容易用肉眼看出波形的失真。
THD要看用在什么场合,比如射频和功放,要求可能完全不同。如果只看波形失真,在功率放大器中一般0.1%的THD可保证基本不失真。在我们的音频功率放大器中,常给出10% THD时的输出功率,此时有削波失真,功率约为无失真时的1.25倍。
您好,不清楚您的输入信号幅度是多少,需要多少增益来达到输出有效值10V。但根据您目前提出的应用需求,推荐高速(高SR>1500V/us,高GBW>50MHz)高输出电流Io>300mA,单端电源电压大于30V或双极性电源大于+/-15V的运放。您可以在下面这个链接中进行搜索,看能否找到满足您需求的运放:
希望对您有帮助,感谢您对TI的支持!
你好,我在实际在测试的时候发现THS6012的地电压随输出波动,但是电源电压相对值不变,所以输出的信号始终可以保证在低于电源电压的3,4之内,所有能够保证有效值为10v,实际达到11v。。。。。。我想请问一下,这是属于THS6012的特有性能吗?对于这个问题我一直不解