vca2617能否作为激光信号的探测放大器?前级耦合应怎样接?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
信号源为APD输出,信号为脉冲信号,带宽50M,幅度为几mv~2v左右,输出阻抗50欧。
VCA2617不合适。从手册上看,这颗运放的带宽只有50MHz,很难保证完全处理50MHz带宽的有用信号。应该换一颗较高带宽的运放。
另外,几mV~2V这个动态范围太大了,你打算怎么处理?是简单放大,还是用其他办法?
前极耦合采用二极管限幅,输出采用它自身的嵌位功能,两级放大级联,大概56db。如果带宽降到20M,这种方案是否可行?
“前极耦合采用二极管限幅,输出采用它自身的嵌位功能,两级放大级联,大概56db”,可否上传一个电路图上来?不是很懂你这句话的意思。“它自身”指2617?56dB增益有几百倍了,这么大的增益去放大几mV到2V的信号?
带宽降到20M也比较困难,可以去官网看看有没有速度更快的运放。
vca2617的输入接成单端耦合,正负端应该怎样接?怎样偏置?另外,调试中,发现噪声很大,不知何原因?