This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XTR116使用过程中出现的问题

Other Parts Discussed in Thread: DAC8551, XTR116

如图,在使用中dac8551不存输出多少,,116输出都会多出4ma,找不到问题在哪,还望技术大神吗解答,万分感谢!

  • XTR116的Iret引脚的地不能直接接到电源的地上,dac8551的地经过Iret进入XTR116回流到电源地上,流入Iret引脚的电流不能超过4mA,否则,无法调节零电平4mA输出。

    看一下Collin Wells的这两篇文章。

    https://e2e.ti.com/blogs_/b/precisionhub/archive/2014/12/09/part-2-two-wire-4-20-ma-transmitters-background-and-common-issues

    https://e2e.ti.com/blogs_/b/precisionhub/archive/2015/02/24/two-wire-4-20ma-transmitters-background-and-common-issues-part-4

  • 可能是因为我截图不完整的原因。图中的24V是外部电源,而iret所接的地是板子上的地,不是24V的地。现在就是将102.4K的电阻去掉之后就正常了,不过不知道原因,不知道这个电阻是否必须要有呢,怎么解释原理呢?

  • Io=100Iin, Iin=Vref/102.4K+Vout(DAC8551)/25.6K. XTR116 的Vref=4.096V,4.096V/102.4K=40uA,40uA×100=4mA,您应该是没有考虑到Vref经过102.4K电阻产生的电流。

    我有点奇怪的是您Vout(DAC8551)为0时输出的电流是4mA还是8mA?

  • z之前没好好研究,只管用了,现在知道什么原因了,Vout输出为0时,电流是4ma,3Q