This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tina仿真模型问题

tina是否可以用pspice模型?还有spice,hspice和pspice模型有什么区别?

  • 搜索了下互联网,发现以下两种版本的阐述比较满意

    SPICE is a powerful general purpose analog circuit simulator that is used to verify circuit designs and to predict the circuit behavior. This is of particular importance for integrated circuits. It was for this reason that SPICE was originally developed at the Electronics Research Laboratory of the University of California, Berkeley (1975), as its name implies:
    Simulation Program for Integrated Circuits Emphasis.
    PSpice is a PC version of SPICE (MicroSim Corp.) and HSpice is a version (Avant!.) that runs on workstations and larger computers. PSpice is available on the PCs in the SEAS PC computing Labs and HSPICE is available on ENIAC or PENDER.

    spice是72年伯克利写的一个电路分析工具,但实际上它只是一个内核,提供核心的算法。一般人要使用各种各样的功能还需要跟它的各种壳打交道,pspice和hspice是比较广泛使用的两种。pspice使用比较简单,常用的有Cadence公司的OrCAD,用的是图形界面。在处理大工程的时候图形界面很容易出错且效率低下,这时候就要用到网单文件(netlist)进行输入(其实pspice也是把图形转化成网单然后才进行计算的),这就是hspice。 

  • OK,谢谢解答。目前我们能用TINA吗?就是官网那种收费版本。你知道怎样将spice模型库整体导入到LIB库中吗?就是我需要直接在软件里面找,不想每次都是插入进去,很麻烦。

  • Chenghong Zhan 说:

    OK,谢谢解答。目前我们能用TINA吗?就是官网那种收费版本。你知道怎样将spice模型库整体导入到LIB库中吗?就是我需要直接在软件里面找,不想每次都是插入进去,很麻烦。

    TINA不需要收费。 有些器件直接给出了TINA reference模型,可直接打开使用,有些器件给出了spice模型,也可直接导入到TINA中。

    或者说如果您确定了芯片型号,直接在型号的产品主页上查看是否有提供TINA 模型。