Other Parts Discussed in Thread: LMH6552, LMH6554
目前在项目中采用LMH6552这颗料,基本满足使用,但是希望用个指标和性能更好的,请TI公司技术人员帮助选型下,具体要求如下:
1、3 dB Small Signal 小信号带宽>1.5GHz(目前的LHM6552的指标);
2、噪声系数不高于LMH6552
3、工模电压最高能接受到+4V(或3.3V)
请TI技术人员帮助选型下,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
是的,带宽大于1.5GHZ的全差分运放中,噪声比LMH6552小的只有LMH6554了,2.8GHz的带宽。
谢谢推荐。
今天按照LMH6554搭建了一个测试电路(按照数据手册的参考图示),其中供电为:+5V,0;差分两路输入的电阻设置为:RF=200欧,RG=100欧,Vcm管脚接地,差分输出端分别串联接入50欧匹配;
用信号源模拟输出了两路差分信号输出给LHM6554测试电路,其中输入c差分信号的峰峰值在20mV,共模电压在1.5V;
目前使用示波器接入测试电路的单端输出观察,发现信号500mV的共模电平
请问下该芯片不是可以通过Vcm管脚调整输出共模电压么,我现在接地后不是输出信号的共模电平应该为0么?为什么会输出这么大的共模电平?如果想让输出共模电平为0,请问该怎样控制Vcm管脚或是其他什么办法?
Vocm是输出共模电压,但是您现在是单电源供电,输出差分信号的平均电压(共模电压)不可能为0。如果需要Vocm为0,建议双电源供电。
有电路图吗?可以发过来看下。
之前也尝试过LMH6552的测试电路和参考电路一样设计,正负2.5V双电源供电。当把Vcm接地后,在LHM6552输出端还是可以观察到约有50mV左右的共模电压,同时改变增益控制电阻Rg和Rf控制放大倍数时,此共模电压会有变化在20-30mV内波动,请问这个原因是什么呢?
反馈电阻是不是画错了?
out+反馈-in,out-反馈+in