Other Parts Discussed in Thread: THS4211, OPA820, THS4215, LMH6609
放大脉冲宽度为50ns,频率为2500Hz,最高幅值6V的脉冲信号,我开始用AD811,实验出来几乎不放大,不知在实际电路设计中还要注意什么?可不可以改用AD8009?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
AD811和AD8009是ADI公司的产品,本论坛是德州仪器技术支持社区,只对德州仪器的产品提供技术支持。
对于你的应用,你可以考虑评估TI的THS4211,THS4215,LMH6609,OPA820等产品。这些产品特点是供电范围大,可以覆盖6V脉冲信号的需求,同时带宽大,可以分辨50ns的脉冲信号。
15V以上可能够呛,THS4211,THS4215最大供电是15V;LMH6609,OPA820最大供电是+/-6V。你的应用为什么要放到这么大?是要驱动后级的大负载?这种高速运放输出幅度太大时,THD会下降得比较厉害,建议放到12V就行。