This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

小白求Ti工程师推荐一款音频功率放大器的芯片

Other Parts Discussed in Thread: NE5532, LM386

音频功率放大器的要求如下:

完成声音信号的放大、滤波和重放(不能使用运算放大器NE5532、集成功率放大器LM386)

系统主要供电模块、滤波与电压放大模块、集成功率放大模块、分立器件功率放大模块等组成。


1、供电电压:±5V~±12V;
2、频率范围:20Hz~20kHz;
3、输出功率:0.5~1W
4、总增益(输出音量)可调,最大200倍;
5、杂音小,失真度小;