最近在使用一款PSD传感器OD3.5-6,资料见附件。
我做的测试电路图如下:
前后选用了跨阻运放 OPA2381 、OPA2354 进行测试。发现两个运放的输出Out1、Out2并没有和Rf1、Rf2的阻值成比例关系。是不是我运放使用方法有问题呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我是试了 Rf 从330R变为10M,但是输出 Out 最大值从 50mV 增大到 110mV 左右
我试着在 4、8脚接上偏执电压 Vr,运放用了OPA2381,发现
增大 Rf,Out 反而变小了,从输出最大 120mV 左右变成 80mV左右(Vr = 3.3V时)。不知道是什么情况额。。
Rf 不变时,Vr = 3.3 时输出最大值会比 Vr = 0时的输出最大值 大。