Other Parts Discussed in Thread: THS4631
各位,我用THS4631做一个峰值保持电路的缓冲级。具体就是接成普通的电压跟随器形式(见图U18)。+/-5v供电。测量时发现输出(pin6)是一个4.2v的高电平。而我的输入实际只是1v的正弦波。单独测试THS4631,将该输入接到(pin3),电路仍是电压跟随器形式。发现输出也没有跟随输入。请问这是怎么回事。另外(pin6)vout-是不是说明它和(pin3)是反相的?急等解答,谢谢大家。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: THS4631
各位,我用THS4631做一个峰值保持电路的缓冲级。具体就是接成普通的电压跟随器形式(见图U18)。+/-5v供电。测量时发现输出(pin6)是一个4.2v的高电平。而我的输入实际只是1v的正弦波。单独测试THS4631,将该输入接到(pin3),电路仍是电压跟随器形式。发现输出也没有跟随输入。请问这是怎么回事。另外(pin6)vout-是不是说明它和(pin3)是反相的?急等解答,谢谢大家。
你这个电路的直流工作点对吗?TRIG控制的晶体管在正常工作下是导通的还是关断的?如果是关断的,那么对于交流信号来说,C73固然可以当成一个交流负载,把交流电流输出转化成电压。但是这里没有直流电流的通路,从13脚出来的直流电流没有通路到地,所以很可能工作时直接把THS的3号引脚直接拉到高电平了。
另外,如果你想单测THS4631,建议测试时和MAX的芯片断开反馈,也就是说,两个反馈里只留一个,断掉芯片间的那一路反馈。还要注意一下1V正弦波的共模,不要太高或者太低。
谢谢你的解答。我在测试的时候没有接晶体管。按照你的意思推测是因为电容上的电压积累所以拉高了THS的pin3么?
另外,我单独测试THS4631,接成电压跟随器,直接在芯片上引出了几根线(整个芯片悬空,没有pcb)。输入1v正弦输出仍然是4.2v高。请问4631的工作情况比较特殊么?您说的共模是怎么回事,要怎么限制和测试?我第一次做模拟设计。还望指教,不胜感激。
1. 是电容上直流电荷的积累,所以拉高了电压。
2. 你单测THS的电路图?可否上传?直接引出的线,芯片地线和输入信号的地线共地了么?
3. 关于共模。比如你输入一个1Vpp的正弦波,如果共模电压在1V,那么实际输入就是0.5V~1.5V;如果共模是0V,实际输入就是+/-0.5V。就是叠加在交流信号上的直流量,这个直流量,可以让芯片正常工作。手册第4页只给出了+/-15V电源下,共模电压范围最差时是-9~11V,你在+/-5V应用时,不要把共模给的太高,应该就可以了。
测试电路如上图。我用示波器做的信号源,设置偏压是0v,这应该能满足吧,可是输出还是4v的。。
我已经共地了。现在的现象是输入向下偏移了500mv。范围是0到-1v,请问这是怎么回事。
好像图片有问题,我的测试电路就是电压跟随器,负载上接了一个1k电阻。测试情况如前。劳驾了
我用TINA仿了一下,电源接反时输入+/-接对时,输出是低电平-5V左右;电源接对输入+/-接反时,输出是3.8V。你是不是把输入的+/-极接反了?检查一下芯片的2,3脚是不是接对了。