This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
看手册上,在正负5V供电情况下,貌似能到3.3V的输出。
我搭的821是10倍的放大,电阻选值和手册略有区别。80改成了75,402改成了390,其它一致。
电源是自己用TPS5430做了一个正负5给821供电(正电压大概4.85,负电压-5),然后发现输出到2.2V左右就开始出现削顶现象了,这是为什么呢?求助各位大神。
从Figure32 来看,当G=10的时候,实际相应输出是从1Vpp~5Vpp。 并且我用TINA仿真了一下,按照Rf=402ohm,Rg=40,G=10的测试条件来看,实际输出大概在4.76Vpp左右。 所以我认为前面电气特性表格里的输出能达到+-3.3V输出是有问题的。