Other Parts Discussed in Thread: INA138
在电路空载时INA138输出端在接上单片机以后会达到0.16V左右,检测电流很不准确,有没其他的大电流检测方案,100mA的精度就能够满足需求了,谢谢推荐。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: INA138
在电路空载时INA138输出端在接上单片机以后会达到0.16V左右,检测电流很不准确,有没其他的大电流检测方案,100mA的精度就能够满足需求了,谢谢推荐。
2mOhm 的电流检测电阻,布局不好的话很容易引入串联电阻,引脚1、2和R1构成的环路要尽量小,OUT输出信号到单片机也很容易引起误差。万用表测过R1两端的电压吗?
您好,需要测量0~200A的电流,INA138输出引脚上电后空接时,用万用表测量点电压为0.023V,接到到MCU的AD采样引脚后电压为0.16V,导致低电流时几乎没有精度可言,目前不确定的时INA138是否可以用来采集200A的电流,在实际测试过程中电流不是很准确。
您好,
您可以看下您MCU ADC输入阻抗是多少,由于R1太大,数量级接近ADC的输入阻抗,改变了等效输出电阻,所以会产生误差,能否减小这个R1试试?
您好,
如果要用这个,需要输出电阻R1比较小,比如10k,这样你的采样电阻需要很小很小,比如变成0.025毫欧姆。
建议用电流互感器采样加运放调理电路来做。