Other Parts Discussed in Thread: TL082
请哪位高手指点一下,有几个问题请教:
1、双电源运放±15V使用过程中,单独的+15V或者-15V突然掉电,只有一组电源供电,运放输出会是什么样?
2、两组电源相差为多少,运放还可以正常工作?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TL082
请哪位高手指点一下,有几个问题请教:
1、双电源运放±15V使用过程中,单独的+15V或者-15V突然掉电,只有一组电源供电,运放输出会是什么样?
2、两组电源相差为多少,运放还可以正常工作?
1. 通常双电源供电是同时上电,如果其中一个掉电,应该会发生latch -up现象。
2. 要看具体型号,每个运放的datasheet都会给出供电电压的范围,在这个范围内就可以正常使用。
1、latch -up对于运放是不是就是把输出电压推到轨电压,比如±15V就会是﹢15V或者是-15V;
2、一般运放只会给出电源是6-36V(比如TL082),没有给出±之间超出多少?
输入共模电压范围指的是运放同相和反相输入端的电压范围。
如果6~36V的电压范围,那么双电压供电就是+-3V~+-18V.
如果是±3到±18,不会是一个是﹢18,另一个是-3的时候,运放的工作还正常吗?
我想问的就是如果一个电源正常的在15V,另一个负电源在跌落,当跌倒什么情况,运放工作
开始工作不正常?”