This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
常用的运放可考虑OPA656,OPA657,OPA659,OPA129等。

你好,我看了一些资料,发现该公式适合于TIA放大 电路,如果是普通的同相运放放大电路,那应该怎么选择合适带宽的运放呢?还有压摆率?谢谢!信号频率还是200KHZ
Hi longjiang,
我想问一下PD光敏管的型号是哪一款?对电路的放大倍数要求是多少呢?
这种光敏管的应用,在选择运放的时候,TIA或者低输入偏置电流的精度运放是首选。
如果考虑普通运放的选型,压摆率的选择,可依据公式SR=2*PAI*f*Vpeak
根据我上面的需求:输入信号频率200KHZ、输出幅度2V,以及压摆率公式SR=2*PAI*f*Vpeak,压摆率约为2.5V/us,请帮忙推荐一款普通运放,谢谢!