振动加速度传感器信号调理电路选取什么放大器比较好,TLC4502可以吗?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
根据您提供的信息,振动传感器的输出是正比于加速度的低频交流信号。初步计算,转化为相关的运放指标为:直流偏置10-14VDC,输出电压动态范围+-5V,带宽15kHz,压摆率要求大于0.94V/us,70uV噪声,在实际应用中需根据您感兴趣的频率范围设置滤波。
初步计算,建议您选择OPA277/OPA2277/OPA4277高精度运算放大器,10uV失调,单电源供电电压可满足4-36V,增益带宽积1MHz,SR 为2.3V/us,15kHz频率范围内噪声幅值约为1uV,满足您的应用。
TLC4502是比较老的产品,且电源轨范围可能不满足,不建议您选用。
LM334是一颗电流型参考源。想请问一下,这种传感器,是加一个电流基准就能产生供电电压吗?
如果是这样,LM334是没问题的。