This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP8640高端放大器误差分析

Other Parts Discussed in Thread: LMP8640, INA282, LMP2021

要求:

uA:0-99.99uA,精度0.1uA。误差1uA

mA:0-99.99mA,精度0.05mA。误差0.3mA

采样高端放大器LMP8640,固定增益50

uA:499欧姆0.1% 低温漂采样电阻。

mA:500mΩ采样电阻

uA最小分辨率:0.1uA*500 *50 = 2.5mV

mA最小分辨率:0.05*0.5*50 = 1.25mV

LMP8640的偏移误差最大1mV。

采样16位ADC采样,以2.5V基准源为参考。请问下我这能做的成功吗?

mA规格:range:0~99.99mA,精度(步进):±0.01mA,误差:±0.30mA;

uA规格:range:0~99.9uA,精度(步进):±0.1uA,误差:±1.0uA;