This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

高频心电信号的sh数据采集



对于TI的参考设计ECG中有提到了Input Bandwidth: 200Hz (ECG signals),其中利用的放大器OPA313与AD转换的带宽都很宽,这个设计可不可以认为高频心电的数据采集?

要想实现带宽在0-2KHZ的心电信号的数据采集应该如何实现?

  • 您好,TI的参考设计是有编号的,请问您看的是哪个参考设计呢?

    心电信号本身是低频信号,心跳一般为60~100次/分,不会超过2Hz,在采样50倍谐波的情况下也只有100Hz.


    ADC选型与具体的设计方案有关,如导联数,软件过采样率算法等。同时ECG设计需满足一定的行业参数标准,满足一定的采样速率。

    TI ECG 方案有 集成的ADS129x系列以及分立的ADS131A0x等,可供您选择。