如题,用在DDS的DA、低通滤波器之后的一级放大,滤波器带宽1M,最后经过放大器输出之后的信号幅度在1Vppz左右,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
供电电压在5V ,输入是差分输入,单端输出,输出电流3mA以上,TL072不知道可不可以
TL072的供电电压范围为+-5V~+-15V,因此单电源供电的话最小10V,所以这款不符合呢。Shoufeng Hu 说:供电电压在5V ,输入是差分输入,单端输出,输出电流3mA以上,TL072不知道可不可以
输入是什么幅值的差分信号?如果有负压,建议双电源供电。