现在想选一款运放,能够处理0.1uA-100uA输入交流信号(基波频率在50hz,希望能够保留谐波在50kHz左右)能够I/V转换到10mV以上,希望能够低噪声高精度的运放不知道可有推荐的运放!不知道opa37可能处理这么小的输入信号
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
OPA37的Iib最大80nA,在选择这种微小电流放大的时候,我们主要考虑运放的Iib是否带来影响, 所以尽量选择Iib<<Iin的精度运放。
另外,您需要的最大输出为mV?那么还需要看下运放的供电电压以及output voltage swing范围。
不是最大输出,是对应输入是0.1uA的时候输出至少是10mv,最大输出可以到5-7v,但是我只需要考虑10mv-1v左右能够保证精度和线性度就行了