请问我在用OPA2134这款芯片做加法器的时候,频率在2M以前是好的,在2M到4M之间信号有放大,在4M以后信号又衰减了,请问这是什么原因?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问我在用OPA2134这款芯片做加法器的时候,频率在2M以前是好的,在2M到4M之间信号有放大,在4M以后信号又衰减了,请问这是什么原因?
Hi hui,
请问在电路中反馈电路的电阻值分别是多大呢?我怀疑是电阻过大,运放寄生电容在2-4MHz使等效电阻减小,增益变大;4MHz处开始衰减是运放本身增益带宽积决定的。
我试着改小了电阻,从10K一直往下调,发觉他还是在2M到4M这里有放大
Hi hui,
方便把电路原理图贴上来嘛?大家一起来分析一下
还是要看下您的电路,输出信号幅值多大?是否是压摆率的限制,OPA2134的SR=8V/us。