1,压摆率在250~700之间
2,轨道轨输出
3,最好是单个运放,没有使能或者关断引脚
其他参数都是次要的,主要依照这三个选型
之前有推荐过OPA355、OPA836,但是都有个关断或者使能脚,不好直接替换(涉及到改PCB)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
下面是根据您的需求筛选出的13个结果,可以看下。比如OPA830可以。确实有些带有PD或者shut down,enable引脚,您目前需要什么封装的?
http://www.ti.com/amplifier-circuit/op-amps/high-speed/products.html#p480=1;1&p22typ=250;700&p78=Out
恩,我们之前找到过OPA830、OPA830-EP,但是发现手册上并没有提到它是轨道轨输出
http://www.ti.com/lit/ds/symlink/opa830-ep.pdf
http://www.ti.com.cn/cn/lit/ds/symlink/opa830.pdf
封装最好是SO8的,SOT23-5的也行
恩,OPA830的话,5V供电,输出最大为4.88V,不知能否接受?
我们是5V单电源供电,为什么强调要轨到轨输出,是因为这个运放输出,是给后面的数字器件的,我们希望运放在工作的时候输出低电压最好是0V,当然这是理想情况,实际我们希望输出低电压的范围是在0~0.15V的范围内,不然数字器件有可能在外部干扰的叠加下误动作,至于输出高电压大于4V即可,所以我们希望知道该运放的输出低电压到底有多低