各位大神好,我使用的OPA2227U(U17)电路上面并么有任何问题,测试也正常,但是发热很大,摸起来感觉烫手估计有个40-50度之间的样子,这个温度我感觉不太正常啊,后级也是跟的运放,没有大负载,为什么会发烫呢,求解答???
后级负载:
求高手解答,急急急!!!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位大神好,我使用的OPA2227U(U17)电路上面并么有任何问题,测试也正常,但是发热很大,摸起来感觉烫手估计有个40-50度之间的样子,这个温度我感觉不太正常啊,后级也是跟的运放,没有大负载,为什么会发烫呢,求解答???
后级负载:
求高手解答,急急急!!!!!
你好, 遇到放大器出现异常发热现象,你可以留意下面两个可能:
1. 放大器的同相输入端和反相输入端之间的实际压差是否比较大,比如超过0.7V。此时由于内部的保护二极管导通,会流过比较大的电流,导致发热;
2. 检查下,放大器是否有出现环路不稳定导致的震荡,此时放大器也可能会比较热;
希望能对你的问题有帮助,如果回答了您的问题,请帮忙点击确认,谢谢!
目前我搭建一个最简单的设计跟随电路,0输入,0输出,正负15V供电,芯片同样会发热,用红外测温仪测试出温度为41度,用手触摸可以感觉到发热,有点烫手,但是芯片还是能够正常稳定工作,我就想请问下,OPA2227U在这种状态是是否就是正常的现象?