Other Parts Discussed in Thread: THS4061, THS3091, THS3001
恳请各位大神推荐一款放大器,能实现以下功能:
1、±15V供电;
2、输入+2V直流电压,经5倍放大能得到+10V直流电压;
3、输入-2V直流电压,经5倍放大能得到-10V直流电压;
4、输入峰峰值为2V、频率为4MHz的正弦波,输出峰峰值10V、频率4MHz的正弦波(要求芯片能处理的频率越大越好);
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi sheng,
推荐您使用THS4061,180MHz 带宽,400V/us压摆率,完全能满足您的需求。
电流反馈的话,THS3001,THS3091也能满足。