Other Parts Discussed in Thread: XTR111
大神们好,我在使用XTR111 4-20mA转换芯片时会有开路的情况,如果开路的话会不会对芯片造成损害呢?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: XTR111
大神们好,我在使用XTR111 4-20mA转换芯片时会有开路的情况,如果开路的话会不会对芯片造成损害呢?谢谢
您的意思是不接负载还是其他情况?个人觉得,如果输出开路,防可以将OD拉高使得输出disable。如果需要恢复正常工作,再将OD拉低即可。
如果输出负载开路,XTR111会通过/EF引脚提供开路提示。
主要风险是,当负载开路时,芯片内部电流检测会认为恒流点没有达到,同时驱动PMOS进入全导通,以增加电流,但是电流因为开路,所以还是为0。此时如果马上接上负载,推测的主要风险是因为PMOS完全通道产生的瞬态电流比较大。所以,标准电路需要加上供输出限流保护的。
/EF引脚可以给MCU提供输出开路提示。
就是要加上XTR111规格书37页的电路。
或者你也可以看看参考设计的电路图,比较接近实际情况:
http://www.ti.com/lit/ug/tidubl9a/tidubl9a.pdf