Other Parts Discussed in Thread: DRV593, DRV8412, DRV594
你好,请问DRV593的驱动方式是PWM输出么?
如果驱动多个TEC,应该采用并联还是串联的方式呢?593的驱动电流最大好像只能达到2A。
还有,593和594的区别在哪里呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如果您愿意采用PWM驱动模式, DRV8412是一颗性价比较高的方案:电流高达3A,并同时可以驱动四颗TEC, 或并联使用电流高达6~7A. 你可以打开以下链接找到所有的有关资料。
focus-webapps.ti.com.cn/.../searchsite.tsp
DRV593/4是PWM输出。593/594的区别是;
The PWM switching frequency may be set to 500 kHz
or 100 kHz depending on system requirements. To
eliminate external components, the gain is fixed at
2.3 V/V for the DRV593. For the DRV594, the gain is
fixed at 14.5 V/V.