Other Parts Discussed in Thread: INA250, INA240
各位好
我想咨询一下,INA250是只能用在直流电流测量吗?能否作为感性负载的高端测量?
现在我使用INA250芯片对汽车电磁阀进行高端电流测量,电流在2A以内,但是上电之后,芯片就被烧毁。目前没找到问题出现的原因。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
INA250不是只能对直流进行测量,交流信号也没问题,能测试电流范围最大为+-15A.
想和您确认下您的输入信号是PWM信号吗?如果是PWM信号的话,不建议使用INA250.
另外,电磁阀的这种电流控制 ,推荐您使用INA240这款。
是PWM信号,我现在使用INA250,上电就烧毁了,电流只有不到1A。原理图和布线都是参考官方Demo板,有可能是因为我的是PWM信号而造成的么?
是的,不建议INA250 用于PWM信号,PWM这种快速边沿脉冲信号很容易将输入部分的ESD打通,这种高频的一致持续的PWM信号会导致INA250在短时间内热量上升的很快。所以有可能将芯片损坏。
因此建议使用INA240 这款:http://www.ti.com/lit/ds/symlink/ina240.pdf
Enhanced PWM rejection provides high levels of suppression for large common-mode transients (ΔV/Δt) in systems that use pulse width modulation (PWM) signals (such as motor drives and solenoid control systems). This feature allows for accurate current measurements without large transients and associated recovery ripple on the output voltage.
很高兴您的问题得以解答,如有任何问题,可随时讨论。