Other Parts Discussed in Thread: LMV981-N
LMV981-N手册里的CMRR指标的test conditions范围Vcm为什么少了中间那0.8V???
CMRR Common mode rejection ratio LMV981-N, 0 V ≤ VCM ≤ 1.5 V, 2.3 V ≤ VCM ≤ 2.7 V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LMV981-N
LMV981-N手册里的CMRR指标的test conditions范围Vcm为什么少了中间那0.8V???
CMRR Common mode rejection ratio LMV981-N, 0 V ≤ VCM ≤ 1.5 V, 2.3 V ≤ VCM ≤ 2.7 V
是的,这个仅仅是测试条件,也是为了说明后面输入共模电压范围的条件,不管是1.8V,还是2.7V供电,可以看到Vcmvr(input common voltage range)的范围是在>=55dB的条件下得到的。 CMRR分别选取了供电电压的两个电压范围段。比如
2.7V供电时,
0 V ≤ VCM ≤ 1.5 V, CMRR 为60dB
2.3 V ≤ VCM ≤ 2.7 V CMRR为55dB