This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教AMC1301输入悬空问题

Other Parts Discussed in Thread: AMC1301

上图中,Iin+,Iin-作为电流采样的输入端口,当接着分流器时,采样正常。当不接分流器时,相当于悬空状态时,输入端口Iin+,Iin-有0.566V的电压,AMC1301的2,3脚也是0.566V电压;AMC1301的6,7脚输出2.5V左右电压。 请问为何Iin+,Iin悬空时AMC1301输入和输出的差分信号不为0V左右,有何改进电流的采样方案可提供。谢谢!

  • 亲;由于干扰和自身偏置等原因,任何未集成内置偏置电路的输入脚都不允许悬空。建议在IN+/-接个几十欧电阻即可。由于电流取样电阻阻值很小,只要并的电阻远大于取样电阻,就不会有明显误差。

    比如,电流取样电阻100毫欧,端口并联电阻100欧。100欧引入误差为0.01%。这个误差通常已经远小于电流取样电阻误差,无需折算即可使用。

  • 请问确定是0.566V而不是0.566mv吗?

  • 首先不建议运放的输入端悬空,这样的确会引起输出不确定状态。

    23引脚间的电压再确认下是0.56mV还是0.566V,不为零是由于输入失调电压导致。

    或者将输入接地,测量下输出为多少。