Other Parts Discussed in Thread: THS3215, OPA2835
您好,我想选一款放大器芯片,可级联的、增益可调、固定增益的都行,我的需求是 工作频率涵盖40MHz±20MHz,增益20~40dB,噪声系数<3.5dB,在TI系统中我查看可级联的放大器的频率最小就到40MHz,想问下各位大神,有没有推荐的TI芯片可以用?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可在下面可编程增益PGA和可变增益VGA 产品选型中进行选型,如果您的信号频率为40+-20Mhz,增益为10~100倍,假设40Mhz的频率话,那么增益带宽积GBW的要求即为400M~4GHz的带宽要求:
http://www.ti.com/amplifier-circuit/pga-vga/products.html#
Hi hai,
450MHz 可以使用,没有问题,不过要达到你要求的增益需要多级级联.