This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

寻找一款超高共模抑制比的仪表运放

Other Parts Discussed in Thread: INA129, INA118, INA333, INA828

寻找一款超高共模抑制比的仪表运放,用于脑电信号的测量,要求超高共模抑制比,超低噪声。

  • 高CMRR的仪表运放,比如INA118, INA333,INA129等,这些最小CMRR都达到了100dB。

    另外,筛选了下120dB~140dB CMRR的仪表运放,结果如下,可参考噪音是否也满足要求:

    http://www.ti.com/amplifier-circuit/instrumentation/products.html#p4min=120;140

  • 亲,INA828可能是最佳选择。建议试试。

  • INA828的共模抑制比确实不错,G=100的时候最小能达到130dB,但我我还是有个问题,就是电路设计的时候,我不是用到单个INA828,我是要起用到23个仪表运放,并且这23个仪表运放的-IN引脚都要接在一起,就用INA129的情况来看,23个仪表运放的IN-引脚接在会导致电路的不平衡,共模抑制比严重下降,实际测量的时候,共模抑制比只能到90dB多点,想问下,有办法解决这个共模抑制比下降的问题吗?