Other Parts Discussed in Thread: ISO122
ISO122/124的输入端采用±15V电源在不要求0~-10V输出的情况下,输出端可以采用+15V的单电源吗
如果两端都采用+15V的单电源是不是只能输入5~10V输出5~10V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ISO122
ISO122/124的输入端采用±15V电源在不要求0~-10V输出的情况下,输出端可以采用+15V的单电源吗
如果两端都采用+15V的单电源是不是只能输入5~10V输出5~10V
VS1和VS2 不一定要相等,只要满足供电电压范围即可。
另外,这款不是轨至轨输出,输出达不到电源轨,您输入是什么幅值的信号?
看到说明书上输出端是可以单电源输入的,想知道输出端可不可以用单电源供电。说明书上的单电源供电电路是要求在输入端的GND提供5V电压作为基准,这样0~10V的输入对应输出会变成-5~+5V,我是想说在这个方案的基础上如果把输出端也改成单电源如果输入是5~10v输出会不会是5~10V。
如果输入端+-15V 供电,输入信号为5~10V,输出单电源15V供电没问题,输出和输入相等为5~10V。
如果输入端+-15V 供电,输入信号为+-5V的话,那么输出单电源15V供电的话,输出就不能跟随输入,负半轴信号处理不了。
也就是说输出端是支持单电源供电的,如果输入端采用单电源供电输入5~10V,输出端也采用单电源供电输出0~5V是可以的吗?如果输出端也采用单电源在输出0V时会不会出现很大的偏移量,或者说输出端的GND引脚也需要给一个基准。