你好。
我这边采用LM4991对单声道音频进行放大。为了实现低功耗,在不播放音频时,功放LM4991设置为休眠状态。
但是在测试过程中,发现功放LM4991一打开使能,喇叭就会有“噗”的声音,请问如何消除这个声音呢?
输入无信号,使能LM4991也一样有这个声音。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
检查电路中主要两个引起pop声的电容大小,一个是输入耦合电容的大小,适当的减小,建议范围0.1uF~0.39uF。
一个是bypass 电容,建议1.0uF电容再搭配一个0.1uF电容。
验证下再使能POP声是否有所改善。