Other Parts Discussed in Thread: LMP2021, OPA335, TLC2652A, OPA734
用OPA129搭了一个很简单的正向放大电路,正负12V供电,输入1mV-100mV的直流信号,但是电路不工作,输出端是10V左右。各位帮分析一下问题所在。谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
像是输出直接饱和了。换块新的试了吗?
电路看不出什么问题。 只是如果被测信号是直流的话,选择运放的时候考虑输入失调电压要远远小于被测信号。OPA129的Vos也在mV等级,这样的话Vos也会随着被放大到输出端,影响输出,但这不是导致输出直接饱和的原因。
换了三块芯片了都是输出10V左右,帮忙推荐其他的失调电压符合的芯片哈。谢谢。
运放是不是震荡了,输入有没有比较大的寄生电容?输出有没有接较大的负载电容?OPA129虽然有最大2mV的输入失调电压,但在1mV-100mV的输入条件下,这个增益应该不会让运放饱和。
目前是在调试情况下,输入是直流电压源,输出接万用表,都是安捷伦的仪表。没有其他的外围电路了,电路很简单都不知道怎么排查了。谢谢
像OPA734,LMP2021,TLC2652A,OPA335等这些低噪声,低Vos的比较适用于低电压信号放大。