R92 = 10K
这样计算的放大倍数是21倍
但是输入一个8mV的电压,理论应该输出168mV;但是实际测试并没有放大,输出也是8mV左右
请问是否我对opa344的理解有误?用法不对?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
测试发现没有虚焊,有没有可能是我选用的电阻太大了,比如200k电阻
这个电路是用来检测电流的,0到5A,输出接芯片的ad转换
还有个问题,opa344和opa345有什么区别,是不是放大倍数大用opa345?