This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA193请教

Other Parts Discussed in Thread: INA193

 如上面电路,检测电流为0~5A。在采样电阻两端电压为0时,输出端测得40mA电压。

请问这是因为什么

  • 40mA电压? 这单位也说得不对
    我看偏置电流也不会引起这么大0偏移, 会不会地线偏差
  • 笔误,是40mV。你说的地线偏差具体指什么,我测试的是直流电机电流,24v,工作电流100ma到2A,因为可能2个一起工作,所以要求测量范围是0~4A
  • Vsense越接近0V, INA193的输出精度越低,您的测试中,Vsens=0V,那么输入共模电压为多少,在INA193 datasheet Page19有针对低Vsense的条件下,输出电压是怎么变化的。可以参考一下。
x 出现错误。请重试或与管理员联系。