AMC1311替代ACPL-C87AT的测试中发现,采样精度,高低温性能测试都已完成,两者差异不大,但在退出工作电压范围时的输出特性有所差异,附件为AMC1311和C87AT在各自退出工作电压点时输出波形的对比,其中蓝色为5V的工作电压,绿色的为AMC1311和C87AT的输出电压,采样的为24V的电源电压,黄色的为一个393比较器的输出电压,当AMC1311(C87AT)的输出电压高于一个1.5V的基准电压时,393输出高电平,低于1.5V时,393输出低电平,从两张图片中可以看出,当5V电压低于4.5V时(图片中Y轴虚线与蓝色相交点的位置),AMC1311和C87AT都不工作,但C87AT的输出电压直接掉下,而AMC1311的输出电压是先上翘(高于基准1.5V了)然后才掉下来,从而导致我的393比较器误动作。这个毛刺产生的原因是什么?