Other Parts Discussed in Thread: INA333
低成本心电仪的信号放大器如何选择,主要看放大器的哪些指标
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好!
下面是主要考虑的几个指标供你参考:
1) CMRR 一般系统要求> 100dB/ G=4, 心电图机一般采用仪表放大电路,对于共模信号有抑制作用,对差模信号(需采集的心电信号)有放大作用。共模抑制比(CMRR),指心电图机的差模信号(心电信号)放大倍数Ad与共模信号(干扰和噪声)放大倍数Ac之比,表示抗干扰能力的大小。要求大于80dB,国际上大于100dB。
2) 等效输入噪声,一般要求 RTI noise: < 30uVp-p / BW:150Hz/ G=4 China 15uVp-p 由于电子热运动产生的噪声,而不是因使用不当外来干扰形成的噪声,这种噪声使心电图机没有输入信号时仍有微小的杂乱波输出,这种噪声如果过大,不但影响图形美观,而且还影响心电波的正常性,因此要求噪声越小越好,在描记曲线中应看不到噪声波形。噪声大小可以用折合到输入端的作用大小来计算,一般要求低于输入端加入几微伏至几十微伏以下信号的作用。国际上规定10≤μV。
3) 输入电阻(Input Impendence > 100Mohms),即前级放大器的输入电阻。输入电阻越大,因电极接触电阻不同而引起的波形失真越小,共模抑制比越高。
建议你看一下INA333的器件。