我目前想用OPA301做一个加法电路,但是根据说明书OPA301好像是单电源供电的,只能接+5V,而我用TINA仿真的时候则必须接+-5V才能正常工作,在实际电路中,我将OPA301接了正负5V供电,结果是迅速发热,无法正常工作,请问到底怎么接电路才是正确的?仿真电路如图所示
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1MHZ以上的方波输入,最大幅值不会超过5V,输入阻抗是10M,电路就是如图所示的一个放大倍数一倍的加法器。那也就是说,可以用+-2.5V供电来实现正弦波的跟随是这样吗?另外我用+-5V供电,芯片快速发热,是否说明芯片以及烧毁?
对的,放大倍数为2,偏置电压为-1,方波是+1V到-1V的幅值。我刚才筛选出了一个OPA656应该是符合我的要求吧?
你好,我按照您的推荐从TI官网购买了OPA656,美国邮过来的,也用TINA仿真过我上图的电路,应该是完全符合我的要求才对。但是今天芯片到货,我焊到了PCB板上,输入是用杜邦线接到信号发生器,输出用杜邦线接到示波器,波形一片混乱,我哪怕用信号发生器给运放一个很小的电压1mv,频率也从50HZ一致调到几百K,输出也呈现溢出的状态,电路完全跟帖子里的电路图一样,请问可能是什么原因导致的?我目前怀疑是用信号发生器的信号线连接输入的杜邦线导致线过长,杂波导致的,但是也不至于导致完全看不出来输出波形才对,而且还是饱和的(即便是输入1mV)。(电路是经过别的运放验证过可以正常使用的,把那个运放取下来之后,焊上去的OPA656)