Other Parts Discussed in Thread: INA118
使用INA118接一个磁阻传感器(相当于4个电阻形成的惠斯通电桥),如图4所示。运放采用±6V供电,放大倍数约为209倍,(Rg=240ohm),但是INA118的输出信号中出现了50Hz的干扰信号(图1和图2)。使用示波器表笔测试INA118的两个输入端,同样发现了50Hz的干扰信号(图3)。这该怎么解决?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: INA118
使用INA118接一个磁阻传感器(相当于4个电阻形成的惠斯通电桥),如图4所示。运放采用±6V供电,放大倍数约为209倍,(Rg=240ohm),但是INA118的输出信号中出现了50Hz的干扰信号(图1和图2)。使用示波器表笔测试INA118的两个输入端,同样发现了50Hz的干扰信号(图3)。这该怎么解决?
Hi,
非常有可能是激励磁阻传感器的电压源不干净,含有50Hz的工频干扰,导致传感器输出信号中含有50Hz工频干扰,进而被放大。
如下图,用TINA进行了仿真,共模干扰信号2Vpp,输出信号中有1.5mV差模50Hz工频信号,被放大之后就会在输出端也出现50Hz工频干扰。
建议选用干净的电源激励传感器测试,看干扰信号时候消除或者削弱。