Other Parts Discussed in Thread: XTR115, XTR116
各位,
我在用多个xtr115做电流环输出的时候,发现一个问题,就是如果这些芯片共用一个24V和地,那么每个芯片输出都不正常,默认输出三十多个毫安,只有每个芯片都用一个隔离的24V才能正常工作。我在网上查有人说需要在各个地上通过磁珠隔离,但是磁珠只是电磁隔离,这个方法我没试,但是管用吗?
这个有没有官方的解释和解决方案啊?
多谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
我测试的地是隔离后的地,也就是给xtr115供24V的地。我现在的临时手段是每一个xtr115都单独供一个隔离dcdc提供24V,4脚输出到受电设备,受电设备的回线接到隔离24V的地上。这样能保证4路xtr115都能正常工作,但是今天测试又发现了一个问题。
我换了一个牌子的3W的dcdc,发现输出电流和受电设备的阻抗有关系。如果我把万用表电流档直接接在xt115的4脚和隔离24V的地,那么输出电流是对的。但是如果串上一个负载电阻,那么这个电流就会变大一点。在200欧姆以下,变化不大,但是超过200欧姆以后,电流增大的很严重,如果用500欧姆的话,输入0信号时,都有三十几个毫安的电流。而用另外一个牌子1W和5W的测试,都没有问题。实在是搞不明白。
这是我一路的电路图,voo0和gnd是我控制电路的电源系统,iso24V是dcdc隔离以后的,4脚输出,回线接到iso24v的地上。