This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello,
在使用LM393时,请帮忙确认下是否可以?
1)LM393输入电流有没有限制?在输入脚输入3mA的电流进去有没有问题?
2)如附件电路图,可以理解为3.3V经过1.5K的电阻直接进去LM393的3脚,看看有没有问题?mcp4017是个10k的滑动变阻器。
Hello,
我的应用是外围电路是3.3串接一个1.5k电阻作为电压基准进入LM393比较器,如果LM393里面输入阻抗特别大,电流远小于3.3/1.5K ma的话是可以接受的。并不希望大电流冲击LM393比较器。