Other Parts Discussed in Thread: TPA3110D2
在应用TPA3110D2时,对照规格书中的公式,发现公式和推荐值对不上,请帮忙说明计算方法。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
查看上述推荐文档,公式为:
Vmax_sg = 4.8 * Vplimit * Zload/ (Zload + 2 * (Rds.on + Rckt) ).
Pmax_sg = Vmax_sg ^2 / Zload * Fpwr.
但是计算功率还是对不上:
Example:Plimit=1.62v
Pvcc=24v,Vin=1Vrms,Rl=8Ω,Rds.on+Rckt=0.4Ω
Vmax_sg=4.8*1.62*8/(8+2*0.4)=7v,Vp_p=14v //------------------输出峰值电压和推荐值一致
Fpwr=1()
Pmax_sg=7*7/8=6.1W //------------------输出功率和推荐值不一致
按照这个计算误还是对应不上:
参考值中:
test condition V Plimit OUT PUT POWER Vp_p
| PVCC=24V, Vin=1Vrms, RL=8Ω, Gain=26dB |
2.94 | 15 | 25.2 |
(VIN.PEAK * Gain / VPLIMIT)=1.414*26/2.94=12.5 对应为Fpwr=0.74,
Vmax_sg=4.8*2.94*8/(8+2*0.4)=12.8v,Vp_p=25.6v //------------------输出峰值电压和推荐值基本一致
Pmax_s=12.8*12.8/8*0.74=15.2W 有效值=15.2*0.707=10.8w //------------------输出功率和推荐值不一致
test condition V Plimit OUT PUT POWER Vp_p
| PVCC=24V, Vin=1Vrms, RL=8Ω, Gain=20dB |
6.97 | 12.1 | 27.7 |
(VIN.PEAK * Gain / VPLIMIT)=1.414*20/6.97=7.12 对应为Fpwr=0.57,
Vmax_sg=4.8*6.97*8/(8+2*0.4)=30.4v,Vp_p=60v //------------------输出峰值电压和推荐值差别较大
Pmax_s=30.4*30.4/8*0.57=65.9W(应该也是到达thermally limited=36.1W) //------------------输出功率和推荐值差别较大