Other Parts Discussed in Thread: THS4551
这是我实际的电路,芯片单电源5V供电,Vcom选取中值2.5V,VG1和VG2是我的电桥差分输出信号作为芯片的差分输入信号,增益为1。此图完全按照数据手册上的FIGURE 76和9.1.6(NG1=2,NG2=5)进行设计。我在用TI高精度数据采集卡进行VM2和VM1电压采集后,发现VM2-VM1的电压一直在向上漂移(十几uV),但是在增益为1的情况下,VM2-VM1应该是一个比较稳定的失调电压值。请问出现这种情况,是因为此款芯片精度达不到uV级别还是我设计的电路存在bug