This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

对时正时负电压信号进行AD转换

Other Parts Discussed in Thread: THS4551, ADS1261, ADS8900B, ADS122C04, ADS9120, ADS1220, OPA211, OPA388, OPA334, OPA335, OPA189, LMP7731, OPA209, THS4521

应用是在高精度传感器信号采集,现在我的信号输出是单端信号,时正时负,要求是用24位精度AD采集uV级别信号,对于我这种信号极性不定的模数转换,应该如何处理,有双极性的24位AD吗,还是先做其他处理?

  • 通常对于这样的情况, 会采用增加偏置的办法转换成单极信号, ADC 后再减去偏置;
    或者转换长差分信号, 采用差分 ADC;
    不过对于这么高精度要求的变换, 损失的精度估计都不小,
  • 因此我现在选择的是THS4551进行差分信号读取,但是发现出现了失调电压的漂移,因此对桥式传感器是否还有更好的信号读取方式?
  • Hi,

    能够输入负压的24位 ADC是有的,ADS1261/ADS122C04/ADS1220都是可以,这些都是delta-Sigma类型的ADC,适合采集缓慢变化的信号,对于变化迅速的信号,推荐使用高精度的SAR ADC,ADS8900B/ADS9120.

    因为是uV级的微弱信号,为了提高信噪比,一般需要经过放大,后采集;如果关心交流精度,则需要选择低噪声的精密运放,OPA211/OPA209/LMP7731 都是噪声极低的运放;关心直流精度,则需要选择失调电压小的运放,OPA189/OPA388/OPA334/OPA335 失调电压都在5uV以下,可以考虑选用。
  • 请问THS4551是否可以用来采集uV信号,因为在实际使用时发现(输出-输入)有十几uV的漂移。具体问题在e2echina.ti.com/.../447851
  • THS4551 本身的offset在常温时最大为175uV。所以不排除是offset造成的影响。

    如果ADC需要差分输入的话,需要先通过精度运放将uV信号放大,再通过THS4551或者THS4521这类全差分运放进行单端到差分转换。