Other Parts Discussed in Thread: OPA549
Hi Team,
我的客户目前想用OPA549来做1路可调输出电压,输出范围1~24V,输出电流8A,负载为容性负载,
1)不知道这款芯片能否带容性负载?
2)输出电压的纹波怎么样?如果供电是27V/100mV的电压,V-为GND的话。
还请帮忙解答,感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1)可以带容性负载,datasheet Page7有几个典型曲线,包括大小信号对于不同容性负载下的overshoot,step response的曲线,可以参考一下。
2)首先建议选择LDO来供电,LDO的输出纹波比较小。 其次您这里考虑的输出纹波,应该是基于容性负载考虑的吧?担心由于带容性负载产生的震荡是吗?
Hi Kailyn,
感谢回复!
1)---如果使用OPA549设计成直流线性供电电源的情况下,其输出带载电容能力如何去评估。(1uF、10uF、47uF、100uF等),这个输出overshoot如何去评估。(实际测试?)
2) ---如上使用OPA设计低压供电,大电流的输出,这个纹波与负载电容的关系如何评估,有没有什么注意事项?(1uF、10uF、47uF、100uF等),容性负载的震荡如何评估和消除。
谢谢!
BR
Susan