This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA549应用咨询

Other Parts Discussed in Thread: OPA549

Hi Team,

我的客户目前想用OPA549来做1路可调输出电压,输出范围1~24V,输出电流8A,负载为容性负载,

1)不知道这款芯片能否带容性负载?

2)输出电压的纹波怎么样?如果供电是27V/100mV的电压,V-为GND的话。

还请帮忙解答,感谢!

  • 1)可以带容性负载,datasheet Page7有几个典型曲线,包括大小信号对于不同容性负载下的overshoot,step response的曲线,可以参考一下。

    2)首先建议选择LDO来供电,LDO的输出纹波比较小。 其次您这里考虑的输出纹波,应该是基于容性负载考虑的吧?担心由于带容性负载产生的震荡是吗?

  • Hi Kailyn,

    感谢回复!

    1)---如果使用OPA549设计成直流线性供电电源的情况下,其输出带载电容能力如何去评估。(1uF、10uF、47uF、100uF等),这个输出overshoot如何去评估。(实际测试?)

    2) ---如上使用OPA设计低压供电,大电流的输出,这个纹波与负载电容的关系如何评估,有没有什么注意事项?(1uF、10uF、47uF、100uF等),容性负载的震荡如何评估和消除。

    谢谢!

    BR

    Susan