使用INA214作高端负载的电流检测,感性负载,RS=1mΩ左右,INA214的V+接5V,REF和V-接地,负载信号(即IN+ IN-)共模电压有12V,输出out接单片机的ADC,如图。
试做过几个样品均是可以工作的,输出正常;但是在小批量生产的时候出现损坏问题,大部分产品的INA214输出有4.3V(比如,差分信号输入IN+ -IN- =0.012V,按照100V/V,输出应该在1.2V左右,实际测得就到4V以上了),只有5%的产品是正常输出1.2V左右,求助:是什么原因造成的。
已尝试:断开其他旁路,只保留驱动电路,和INA214电路,更换过多次INA214,刚换上去的时候是好的,上电工作就损坏,明显特征测IN+/IN-对GND的电阻,好的情况下该电阻值=1.2kΩ,损坏的情况下该电阻值=110Ω左右。