This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA549电路输出8A电流,接不同负载测试。输出电压为1.364V时,需(V+)-Vo>5.5V,才能输出8A电流,超过理论值(V+)-Vo =4.3V;当输出电压为2.9V时,满足(V+)-Vo =4.3V关系

Other Parts Discussed in Thread: OPA549

            在测试单片OPA549电路性能时,有如下疑问,能够帮忙协调相关支持FAE帮忙解答或现场讲解!

1OPA549电路设置输出电流的限流电阻时,理论上867Ω,最大输出电流8.97A,实际最大输出电流8.16A,这是什么原因?

2 OPA549电路输出8A电流,接不同负载测试。输出电压为1.364V时,需(V+)-Vo>5.5V,才能输出8A电流,超过理论值(V+)-Vo =4.3V;当输出电压为2.9V时,满足(V+)-Vo =4.3V关系。

      当输出8A电流时,当输出电压低于哪个值时,不满足(V+)-Vo =4.3V关系?

  • 亲;你这是在PCB板上测的还是飞线测试?请上传测试板照片并详细指出测试工具和测试位置、波形。

  • 注意两方面:第一,OPA549的电流最大输出10A, 连续输出8A。 因此我们不希望长时间的输出10Apeak 值,这样有可能使得OPA549 的性能降低。
    第二,本身这是一款高压高电流输出的,所以一定注意散热。 输出电流降低很有可能是散热不良的限制。