This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

opa548输出问题

Other Parts Discussed in Thread: OPA548

如下电路±5V供电,E/S 通过1K电阻接到V-。输出未使能。上电后V量测V0确有有-4V左右电压,IN-有-2V左右,求解答

通过信号控制光耦打开,E/S信号0V左右,输出使能。IN+前段是DAC输出0V。可以看到开关电源±5V电压都上升了600MA左右,此时V0悬空

  • 从您的描述来看,E/S引脚功能失效,disable输出的时候反而却enable 输出了,并且输出结果也是正确的。
    方便换一块OPA548试试吗?关于开关电源上升的问题,我建议断开外围电路,只测量OPA548.