This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

放大器低噪声问题

工程师您好:

        我要用传感器测量一个指数衰减的信号,假如系统的带宽是100KHz,如果噪声在这个带宽内的RMS值是200uV,那么我的信号衰减到什么程度就不能分辨了?如果我将传感器的噪声谱密度从1KHz后开始降低,那么噪声是可以降低吗?此时信号衰减进入噪声区的时间是否可以变长?

  • 您好

    1. 当噪声的峰峰值大于1/2LSB时,有用信号就不能被分辨。如果要确定你的信号衰减到什么程度就不能分辨了,需要确定系统ADC的位数,以及ADC的噪声,综合整个系统的噪声去分析。

    2. 传感器的噪声谱密度再被生产出来时就已经确定,是不能认为的降低的。理论上分析,噪声谱密度降低,有效带宽内噪声会降低。

    3. 噪声是服从高斯分布的,1KHz以内也是有噪声分布的,所以不管你的信号何时衰减,都会有噪声区的存在。

    希望以上解答可以帮助您!