Other Parts Discussed in Thread: OPA170, TLV2370, OPA188, OPA180, OPA172
各位专家:
关于OPA170在采用单电源供电时候,比如15V单电源供电,输入信号0-10V,输出是否可以0--10V输出。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
OPA170的输出范围可以参考datasheet Page10的电气特性Voltage output swing from positive rail最小值为115mV, Voltage output swing from negative rail 最大值为70mV,也就是说0~15V单电源供电的话,输出不能完全轨到轨的话,至少为70mV~14.895V。 所以输出10V没问题,可能不能完全接近0V。